This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a problem when trying to connect EV2400 to our board that has BQ27742-G1.
While if I am using the board EV2400 connected to the BQ27742EVM the connection is fine.
When opening bqStudio selecting the target from the list (gauge-> 0742_1_03-bq27742G1.bqz)
I got the following message:
"The detected device is not compatible with this application!
Some actions could cause the device to lose communication permanently and enter an unrecoverable state.
Proceed at your own risk.
Select OK to continue, Cancel to close the application."
Selecting OK, I can see that it detect the device, with voltage, charge etc., but after few secondo it disappear and remain disconnected.
EV2400 Firmware: Version 0.32 (same was happening with version 0.28)
bqStudio version 1.3.101
Chemistry version 1006
IC address: 0x55
If I am using my microcontroller to connect to the BQ27742 it works fine.