Hi,
I'm reading the SNVA829. In the section 4 of this doc, it says the Rsense in series with the output will increase the loss. But when using a Rs to sense the output current, it will also increase the loss, right? As shown in section 6, the current flows into Rs will be 2*Iout. So, if Rs is chosen larger than Rsense/2, the loss increasing will even worse than the traditional method.
Thanks.