Dear friends.
We need to monitor the voltage windows in the cells of a electrolyzers stack. Number of cells will be around 100, so it means 100 voltage in series. The voltage of one individual cell should be normally 1.8 - 2.0V. Then, the total voltage of the stack is 180 - 200 V.
We found TPS3704Q1 while searching for ICs, but we don't know if it is possible to use it for messuring 100 cells, for example if 4 voltages can be monitored with one unit, then 25 units for monitoring the full stack. Or which of your products would be better for our goal?
We don't need balancing features, etc., as this is not about batteries. We just need to create an alarm if one of our 100 cells has a voltage lower than 1.7V or higher than 2.5V.
Kind regards