I'm working on implementing a PFC pre-regulator based on the example circuit in the UCC28056 datasheet and the UCC28056BEVM-296 evaluation module. I don't understand some of the design choices and I'm looking for some help.
In the UCC28056 datasheet, figure 36 shows an example schematic. There are three resistors in parallel for current sensing - RCSa, RCSb, RCSc. Their values are 0.13, 0.13, and 453k. I don't understand why the 453k RCSc resistor is included. It seems that in parallel with two 0.13 ohm resistors, it has negligible impact on the result.
Thanks!
Thomas