Other Parts Discussed in Thread: TPS62A01
Hello,
For context, I plan on using the TLV62085RLT voltage regulator to power a device with a stringent voltage regulation requirement of +/-3%. The datasheet of the regulator notes that the feedback regulation voltage (VFB) is spec'd for a min of 792mV, a nominal of 800mV, and a max of 808mV at Tj = 0C to 85C. However, on WEBENCH, the tolerance is set to 20mV regardless of the regulator's junction temperature.
1. What is the reason for the difference in tolerance between the datasheet and the simulation tool?
2. Is the tolerance on WEBENCH for the entire junction temperature range of the regulator (-40C to 150C)? In some cases, the junction of the regulator I'm using will approach 90C.