This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for Battery Charger for LiNiMnCo Coin Cell

Other Parts Discussed in Thread: BQ25618E, BQ25628

I am looking for a Li+ DC-DC buck charger for a 300mAh Lithium nickel manganese cobalt oxide coin cell battery. Input is 9-12V, output is 3.3V, load is very small ~8mA but needs to be very efficient. Powerpath device is preferred. BQ25618E appeared to be a good fit although it doesn't seem like it might meet the 4.2V for 3 hours requirement. Here are the requirements from the battery:

  1. Charge the battery in a temperature range of 0°C to + 45°C. b. Charge the battery at a constant current of 0.5C until 4.20VDC±0.03VDC per cell is attained. Charge rates greater than 1C are NOT recommended. (C: Rated Capacity of Battery) c. Maintain charge voltage at 4.20VDC per cell for 3.0 hours (recommended for maximum capacity). * Use a constant current, constant voltage (CC/CV) lithium-ion (Li+) battery charge controller. * Do not continue to charge battery over specified time.
  2. Recommended cut-off voltage to 3.0VDC. Recommended maximum discharge rate is 2C at constant current. b. For maximum performance, discharge the battery in a temperature range of –20°C to + 45°C.