Other Parts Discussed in Thread: TPS563201,
Hi team,
Can you please take a look into the attached schematic with TPS563201 to comment if they can reuse passive components with TPS561201?

Best regards,
Hayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shuai,
Customer's in/out is 14.5Vin_max, 5Vout, 600mA max. When I substitute these value into equation (4) to calculate Iripple
Iripple = 5/14.5 * (14.5-5) / (3.3u * 580k) = 47.5/14.5 * 1/(3.3*0.58) = 1.71A
So Iripple/2 = 0.86A. Because minimum current limit is 1.2A, customer should change the inductor to higher value, correct?
When change to 4.7uH, Iripple/2 = 0.60A. It is few margin.
When change to 6.8uH, Iripple/2 = 0.41A. It is guessed as OK. But is there any concern?
Overall, is there any mistakes on what I calc?
Regards,
Hayashi
Hi Shuai,
I read the datasheet and found below, which seems confliction with your comment
If the monitored current is above the OCL level, the converter maintains low-side FET on and delays the creation of a new set pulse, even the voltage feedback loop requires one
I understands as below
After HSFET On-time, LSFET will on and detect overcurrent immediately because the switch current (Iload + Iripple) exceeds OCL threshold (1.2A min). Then LSFET on-time is longer than Duty_off / fsw since LSFET keeps on until the overcurrent condition is removed. When the device repeats it in every switching period, the output voltage will be lower due to longer off-time.
Is my understanding correct?
Regards,
Hayashi
Hi
Your average current is just 0.6A. When inductor current from 1.7A to 1.2A, OCL protection will be triggered, LSFET will have the highest priority to turn on.
One current be lower than 1.2A, protection logic will be canceled. The turn on/off behavior of LSFET will determined by normal logic. It will not affect the duty cycle.
Assume it doesn't exist OCL protection, the behavior is the same.
If customer still have concern, it is better to use 6.8uH. It is ok at my side.
Shuai