Other Parts Discussed in Thread: UCD3138OL64EVM-031
Hi,
When AD0 is used for the address pin sampling, the corresponding AD sampling value is higher than the theoretical value. After checked the waveform that the AD0 pin voltage value is higher during sampling process. At first , we suspected that it was because of sampling value of the previous channel. Later we found that only samplling this channel would have such a problem. It is worth noting that the voltage corresponding to our channel is 150mV. Before AD sampling, the voltage is 0.15V (10uA*15k), but the voltage rises to 0.17V when the sampling is enaled.May I ask, what causes the high AD value? Any good suggestions? Thanks.