Good afternoon,
We are successfully booting up and there is not any noticeable heat generation, but we are getting a flashing STAT light (fault condition) and the PGn signal is only active in a specific voltage range within a few volts of the battery.
This is a new battery pack, so I am waiting on confirmation from the vendor on the thermistor details, but the voltage on TS looks to be in rage (2.2 V). However, VREF is also 4.1-4.2 V instead of the expected 3.3 V.
Do you have any thoughts?
Thank you,
Kris