This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51050B: BQ51050B

Part Number: BQ51050B

I have a bq51050B design that works well.  The resistor settings based upon Figure 32 in the datasheet, has R1 = 470, Rterm = 2.4k and Rfod = 215.  I wanted to increase the current when I started using a 7Ah battery.  I made two changes: R1 = 100 and Rterm = 1.2k. After I made this change, the circuit stopped charging when the battery voltage reached 3.92V.  I tried several different values for R1, but was never able to get a complete charge up to 4.2V, unless I set R1 back to 470.  I also tried a 1000mAh battery and it showed the same behavior. Do have any suggestions?  

I attached two pictures showing the voltage and current graphs to better understand the situation.