Hi,
A quick clarifying question about BQ25120A operating modes. Table 10 in datasheet shows that VOVP is inactive during ship mode. Does this mean that there is no overvoltage protection and PMID would see whatever voltage is applied to VIN? Or does it mean that the OVP hardware is irrelevant in ship mode because PMID is disconnected from the input regardless, so the overvoltage comparator is disable to save power?
Put another way: If the end user tries to wake the device from ship mode by plugging in a 12V power supply, will the input voltage propagate through to PMID and any downstream loads?
Thanks,
Carl