This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90320: Vout margin +/- 3% resistor calculation

Part Number: UCD90320


Hi ,

Can you sanity check the correct resistor value network for +/-3 % for following example :

Controller (LDO) device :

TPS7A5401

Vout = 0.90V 

Vin = 1.20V

R1 = 12.4K

R2 = 100K

VFB pin is driven by UCD90320 Margin/GPIO (pin E12) through R3 = R4 = 178K , C1=1000pF. Are  R3, R4 values correct to achieve 0.90V +/- 3% ? 

Need a sanity check on calculation result, Please advise.

Thanks

Kam.