Is it possible for TPS563200 to output +5V@3A and -5V@500mA from input 12V?
Wether the below schematic is OK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jerry!
Second SH is wrong. If you want a negative output, you can use buck converter to construct a buck-boost converter.
Shuai