This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25616: Q4 (BATFET) OFF state

Part Number: BQ25616

Hi team,

Can I check when the Q4 FET is OFF? Is there any other state to shut off the Q4 FET?

1. CHG_EN =Disable

2. CHG_STAT = L (I know it is output, want to confirm if the indicator is relating BATFET or no switching)

3. No battery connected

Best regards,

Hayashi

  • Hayashi,

    The BATFET may control the current flow bidirectionally.

    1: /CE: When charge is disabled, the current can’t flow from SYS to BAT (charging), but the current may flow from BAT to SYS (discharging).

    2: Can't tell BATFET status.

    Already answered the same question on 3/27/23 email.

    Thanks,

    Ning.