If the LD pin level is higher than 1.45V after the BQ76952 receives the shutdown command, will the BQ76952 wake up again?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the LD pin level is higher than 1.45V after the BQ76952 receives the shutdown command, will the BQ76952 wake up again?
Hello,
Correct, the device can be waked up from shutdown if the LD pin has a voltage higher than 1.45V (typical voltage). I applied 1.35-V on the LD pin and it woke the device (it depends on each device).
The device will remain awake if there is a LD voltage and the command for SHUTDOWN is received. It will go into SHUTDOWN once the LD voltage goes below the LD wake threshold.
Regards,
Jose Couso