Part Number: TPS272C45
Other Parts Discussed in Thread: TPS2H000-Q1
Hi,
I see on the datasheet that the max Rclim value is 28.2k, which results in a current limit of ~727mA.
Rlim = Kcl / Icl --> 28.2k = 20.5 / Icl --> Icl = 727mA
For my application I require the channels to be current limited to 500mA or below (Rlim = 20.5 / .500 = 41k) . If I place a Rclim = 41k to produce Ilim = 500mA I have two questions:
1) will the device be able to current limit to this lower level?
2) If so, how will the accuracy be impacted? (I am willing to compromise on accuracy in order to achieve this current limiting)
Thanks!