Hi everyone,
I have a circuit that uses a LMR62421 as power supply, I show you the design:
VBAT1 is the voltage of a battery and 7V should appear on the output, but VIN appears on VOUT, it is as if the circuit did not work, I replaced the LMR62421 and I am using an oscilloscope to see the PWM signal of the SW pin, but it does not exist no signal, i can only see the VIN voltage which also appears on SW, what could be happening?