This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2840: TI Webench Power Designer Simulations Fail

Part Number: LM2840


I created a design for the LM2840X in TI Webench using the following settings

Vin: 24V

Output: 3.3V @ 0.05A

Max Ambient Temp: 85C

Webench successfully creates a schematic but when I try to simulate, only the Bode Plot simulation works. The Load Transient, Input Transient, and Steady State simulations fail.

Bode Plot simulation works but the other three simulations fail

Error message shown at bottom of window when simulation failed