Other Parts Discussed in Thread: GPCCHEM
Hi
I just ordered the BQ34Z100EVM board. I have a few battery packs I'd like to use it with, namely:
-4 Series 3 Parallel Lithium Thionyl Chloride (primary, 29 Ah per cell capacity, 3.67V 800mA max constant current)
-4 Series 3 Parallel Lithium Sulfuryl Chloride (primary, 32Ah per cell capacity, 3.93V 2000mA max constant current)
I don't see any matching models in the Chemistry tab in Battery Management Studio. I asked TI support for help, and they sent me to this forum to ask for help. Can you please suggest what steps I should take in order to be able to use the BQ34Z100EVM board with the batteries I stated above, or point me to any resources I could use? Thanks a lot!
Kind regards
Rob