Other Parts Discussed in Thread: LMG3522R030
Hi,
Is there any characteristics curve graph for this part number and what is the PWM input range.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is there any characteristics curve graph for this part number and what is the PWM input range.
Hey Sivaranjani,
The LMG3522R030-Q1 is the automotive qualified version of the LMG3522R030. The LMG3522R030-Q1 isn't fully released yet; because of that the data sheet is not finalized and does not include all of the graphs and figures. The LMG3522R030 is fully released and the data sheet for it is finalized and published. I've attached the link below to the LMG3522R030 product page which also has the data sheet on it.
https://www.ti.com/product/LMG3522R030
Also to add, the PWM input range voltage from the Absolute Maximum Ratings section of the data sheet is defined as -0.3V - 20V. Please keep in mind that our devices include an integrated gate driver.
Best,
Kyle