This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggest a suitable controller IC

Dear Team,

We are designing a non-isolated DC-DC Buck converter using external discrete components such as MOSFET,Diode, Inductor & Capacitor.

Input & output requirement details,

Input voltage =320V to 360V

Output voltage=0 to 300V (Adjustable)

Output power (Max)=2kW.

Please suggest the suitable buck controller IC.

Thanks in advance,

Regards,

Vairavan P