This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79616-Q1: OTUT_THRESH register setting

Part Number: BQ79616-Q1

The BQ OTUT comparators use the ratio of the (GPIO voltage/TSREF voltage) to determine OT and UT faults. For an OT_THR register setting b00000 (which is 10% from the discussion in the related link), how do I translate 10% to a temperature value? The firmware calculates the NTC value based on the GPIO voltage and TSREF voltage. These voltages are calculated applying the scale factors to the GPIO and TSREF register readings.

Thanks,

Priya