Other Parts Discussed in Thread: TPS23861, , ,
Please Suggest a Part number for a single port PSE IC with 12-47V support Same AS TPS23888
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Karthikesh,
Which 802.3 spec (af, at, or bt) and highest class power (from 0 through 8) is needed for your application?
If you're looking for a PSE similar in features to TPS2388, then I recommend either TPS23861 or TPS23882(B), I'll include the link below.
TPS23861 is a Type-2 (2-pair only), 802.3af PSE devices that comes with 4 channels and includes autonomous mode (no host/MCU required for operation).
Thanks and Regards,
Raymond Lin
Hai Raymond,
I am looking for 802.3 af/at ,type-2, 2 pair (POE+) IC for handling a single channel . Whether any IC available with same spec for non standard POE voltage of 24 and 12V.
Hi Karthikesh,
same spec for non standard POE voltage of 24 and 12V.
Just to clarify, are you looking for a PSE solution that can output 12V-24V on the VPWR line to the RJ-45 and Ethernet cable? If so, unfortunately we do not have any discrete/integrated PSE solution that can output that low of a voltage range since it will trigger UVLO (Under-Voltage Lockout). The typical VPWR operating range is from 44V-57V is we highly recommend to keep VPWR within this range. It's possible to use an adapter or some other system solution to achieve that voltage range but our PSE by themselves will not be able to.
For Type-2, 2-pair PSE follow 802.3af/at specs, I recommend TPS2388 or TPS23861. TPS2388 runs in either manual or semi-auto mode (requires host) and includes 8-channels. Reiterating the features of TPS23861, includes 4 channels and also has autonomous mode (no host/MCU required for operation) along with manual, semi-auto and automatic modes (these modes require host). For your application, I would recommend using TPS23861 if you don't need to support that many channels/ports.
Thanks and Regards,
Raymond Lin