Hello,
we need the input capacitance (Cin) and the acquisition time (t acq) of the Main ADC of BQ79656.
This information is mandatory to select the bandwidth of the input filter of the analog-front end. We don't want to use the recommended BW from datasheet as it is too low for our application.
We need to monitor as much fluctuation of the voltage cells as we can (higher signal BW) so the recommended BW with the very low cut-off, does not fit for us.
We need Cin and t acq values in order to calculate the best trade-off of the filter BW in combination with the given sampling rate. So it is all about settling time calculation of analog front-end, taking into account kick back effects.
Thanks in advance,
Argyris