Other Parts Discussed in Thread: TPS40057
Hello TI experts,
My customer now check the schematic of TPS40055. Could you review the schematic first?
and they have a problem that sometimes the output is not detected even input power is applied.
they do not use PR57 resistor, so COMP(pin8) is floating.
is it necessary to connect COMP pin to operate TPS40055? what happens if COMP pin is floating?
I attach waveforms of startup.
: Upper line is SS pin. yellow is fault operation and white is normal operation.
Lower line is 5V output. sky-blue is fault operation and white is normal operation.
: This is the current consumption when the fault is detected in startup.
Please check this issue. Thanks.
Best regards,
Chase