This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z110: BQ34Z110 design query

Part Number: BQ34Z110
Other Parts Discussed in Thread: BQ34Z100, BQ24650

Hi 

I have a query need your help.

There is a device use two 12V lead-acid batteries, one main and one backup. Use two BQ34Z100 chips. Communicate with Android system with I2C. The charging path of the BQ24650 solar charging chip has automatic switching, and the discharging path is also through automatic switching. Does it feasible?

Can I use two USB to I2C or USB to UART and then to HDQ?

In the following Technical Reference Manual

9.6 Using UART Interface to HDQ
An implementation option for HDQ is to use a UART. An advantage to using the UART is that if the
UART is handling the communication and storing the results in a buffer, host processor interrupts during the
communication do not affect the timing of the HDQ communication with the HDQ target. Use of the UART for
HDQ communication requires that each word sent to or received from the UART is only a single bit of the
HDQ data or address. The procedure is to set the UART baud rate to 57,600 with no parity and two stop bits.
This yields a data word with 11 bits total (start bit, eight data bits, and two stop bits). At a baud rate of 57,600
(17.3 μs per bit), this is a total communication time of 190.9 μs and meets the required HDQ bit timing of 190
μs minimum. If data of 0xFE is sent to the UART, the transmitted data is low for 34.6 μs and then high for
the remaining bit time and is interpreted by the HDQ target as a 1. If data of 0xC0 is sent to the UART, the
transmitted data is low for 121.5 μs and then high for the remaining bit time and is interpreted by the HDQ target
as a 0. When data is sent to the host from the HDQ target, the received data could be interpreted as either
0xFE or 0xFC if a logic 1 is sent, or either 0xF0, 0xE0, 0xC0, 0x80, or 0x00 if a logic 0 is sent. A simple test
of the received data determines the received data bit. If the received data is greater than 0xF8, the data bit
should be interpreted as a logic 1, and if less than or equal to 0xF8, the data bit should be interpreted as a
logic 0. This analysis assumes the UART samples the received data approximately half-way through each of the
17.3-μs UART bit times, and that capacitive loading on the HDQ line may delay the rise time of the data a few
microseconds.
Note that the TX and RX of the UART must be tied together because HDQ is a single-wire interface. In case the
TX output is not an open-drain output, it needs to be converted to an open-drain output, as shown in Figure 9-5.

Waiting for your reply.

Thanks

Star