Can I/should I use a TP25750D to manage power delivery on an USB-C upstream facing port power and data port?
i.e. I want to negotiate 15V @ up to 3A from the DFP and I want a data connection.
I think everything on the data sheet assumes no data role.
If I can do this then:
Can I use the GUI to setup 'Cable_Orientation_Event' to control a GPIO to control a superspeed MUX?
Can I use 'AttachedAsSink' to indicate via GPIO that a PD contract has been negotiated and that power is available?
If power is not available, is there an event or combination of events that can be used to indicate that a cable is attached and that it is sensible to try data communication?
Is more information about 'Dp_Dm_Mux_Enable_Event' available?
Is more information about 'UFP_Indicator_Event ' available?