This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1117: Design required to convert from 12V to 5V

Part Number: LM1117

Can you please provide circuit design to get the below mentioned output?

Input range :12V

Required fixed output: 5V fixed output

Iout: 0.7A

  • Hi Keerthana,

    Use this schematic as a reference. R1 = 121 ohms, R2 = 1.05 kilo-ohms. 

    Be sure to follow the datasheet guidelines on input and output capacitors.  Ceramic capacitors by themselves will not work as Cout, unless you place a series resistor at least 0.3 ohms.  Dry tantalums may be fine if the ESR is high enough, and aluminum electrolytic capacitors should be fine.

    Thanks,

    Stephen