Hi, I have followed the steps for "Achieving the Successful Learning Cycle," and as a result, the "Update Status" changed to 0x0E. Then, I exported optimized *.GG file, changed "Update Status" to 0x02 and "Cycle Count" to 0 in the file. After that, I programmed the original SENC file and imported the *.GG file back. However, at the final step, the charge and discharge FETs are disabled. I do not understand how to activate them in the production line, should I send IT Enable command, just like I did during the learning step?