This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2521: Recommended operating conditions for VOUT

Part Number: TPS2521

Hello,

I would like to ask you about the recommended operating conditions for VOUT of the TPS2521.
The data sheet has the following red frame description.
If VIN is 5V, will 5V+20V be MAX?
Also, please tell me the meaning of 23V.

Best regards,