I am using some LMZ10503 regulators for 5V to 3.3V, 3.3V to 1.2V, and 3.3V to 1V conversions. We noticed in the lab that the outputs seemed to be tied to the input voltage rails. For example with the 5V to 3.3V conversion we were seeing 5V on the output. Similar with the 3.3V converters.
The datasheet routing guidelines mention having output resistors/capacitors on the same side of the board as the LMZ part, but ours are on the opposite side of the board. Would that cause this issue? We white-wired our feedback circuitry to the top of the part and that seemed to correct the issue. Any thoughts?