Other Parts Discussed in Thread: LM5155
Hi team,
May I know if you have below temperature-Vsense curve? 100mV and 190mV corresponding to Vsense under which condition? Thank you
Thank
Scarlett
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ji,
If no curve, can you suggest if any relation between Vsense and temperature? when the min and max will occur? Is it just from device part to part variation and no link with temperature??
Thank you
Scarlett
Hi Scarlett,
Like Feng already mentioned, I am afraid we have no detailed test data on any Vsense-temperature dependencies.
From the datasheet, it looks to me like this min and max Vsense value are the worst case limits over all scenarios, including full temperature range, voltage/current ranges and part variance. Therefore, I would assume temperature is only one of several factors that could influence the Vsense voltage.
Best regards,
Niklas