Team,
Can someone clarify the footprint/package of the TPS63020? The first page of the datasheet (under FEATURES) mentions that the TPS63020 is available in a QFN-14 package. However, the mechanical data at the end of the datasheet is for a VSON (DSJ) package. Also, the only orderable options online is for the VSON (DSJ) package. Is VSON (DSJ) the same as QFN-14 package? Thanks, Fern