Other Parts Discussed in Thread: BQ40Z50, EV2400, , BQ24610
I have a configuration of 3S battery with bq40z50 as a fuel guage.
I am using ev2400 with bq studio to configure the ic. here are the register values
* Created: Thu Apr 13 02:20:45 CST 2023
*
* Format: Register Name tab Character,\t Hexadecimal register value.
* Device: bq25700A
* BQZ Container: Charger_1_00-bq25700A.bqz
*
Charge Option 0 040C
Charge Current Register 0280
Charge Voltage Register 3130
OTG Voltage Register 2940
OTG Current Register 0400
Input Voltage Register 3640
Minimum System Voltage 2400
Input Current Register 0A00
Charge Status Register A004
Prochot Status Register 0000
Input Current Limit In Use 0A00
VBUS and PSYS Voltage Read Back B8FF
Charge and Discharge Current Read Back 0000
Input Current and CMPIN Voltage Read Back 0000
System and Battery Voltage Read Back 9292
Manufacture ID Read Back 0040
Device ID Read Back 0079
Charge Option 1 1258
Charge Option 2 0235
Charge Option 3 0800
Prochot Option 0 4A54
Prochot Option 1 4900
ADC Option A07F
The battery does not charge with this config. However the system voltage reads out as 12.2V which is the battery voltage.
When battery is removed there is no system voltage
here is the schematic. Only thing i am not following the schematics guide on is the ilim_pin resistors. However i disabled external_ilim in config