Hi,
Good Day.
I need some information about PIN 5 of the device. The pin is left floating on the PCB and on the datasheet is written that to have the device on is possible to leave the pin floating (open). In the datasheet is also written that to have the device on the voltage on the SD pin has to be less than 0.6 V. The question is: If the pin is left floating how I can guarantee always the voltage below 0.6 V? Is it present an internal pull-down?
Please advise. Thank you very much.
Best Regards,
Ray Vincent