This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256403: Are there any conditions other than "OCP3 threshold" to enter OCP3 operation?

Part Number: UCC256403


Figure 1 shows OCP3 operating waveforms. Figure 2 shows OCP3 not working.

The ISNS pin (ch2) in Fig. 1 has an average value of 0.403V per cycle, so it corresponds to "OCP3 threshold min 0.40V".

Figure 2 is also 0.449V, so it should correspond to "OCP3 threshold min 0.40V". However, Figure 2 does not show OCP3 operation.

In addition, the operation to pull out the FB terminal from another circuit is implemented.

fig.1

fig.2

ch1: output voltage ch2: ISNS pin voltage ch3: HO pin voltage ch4: output current

thank you.