Hi, I want to design a battery charge circuit for 2 lithium battery; however, the DS omits some calculation or information.
- TS --> DS states that is recommended to use 103AT-2 10Kohms as thermistor, but when I read the design procedure, I only see in the schematic a voltage divider
- ILIM_HIZ --> this pin is to set the current input limit of the circuit, right? And the formula is Vilim_hiz = 1V + 0.8*ILIM. How is a good current limit for a 2S charger configuration? How can I infer if a 500ma or 1.5A is a good current limitation.
- Vsys --> how do I know the output voltage of the system? if I have 2S configuration, that mean Vsys would be 7V - 19V?