Hi team,
My customer want to use TPS92682 in two conditions as below, could you please help to evaluate the application possibility and limitation?
1. Configurate the 2 channels as: Buck-Boost CC mode. Vin=7~18V, Vout=50V, Iout=1A. So total maximum output power is 100W. What factors determine the maximum output current in CC mode?
2. Vin=7~18V. Configurate channel 1 as Boost CV mode, Vout=55V, Ioutmax=1.6A. Configurate channel 2 as Buck-Boost CC mode, Iout=1.2A, Vout=60V. Could you please suggest if one channel is Boost CV, one channel is Buck-Boost CC, how to determine the maximum output power for each channel?
Thanks for your support!