Part number: TLV74333PDBVR
We have developed a battery-powered board with TLV743P LDO.
The input of the LDO is supplied by the battery, and when the battery is not inserted, it is directly connected to the battery charger IC TP4056-4.2. The enable pin of the LDO is shorted with the input voltage, and 1uF of capacitance is placed at the input and output of the LDO.
When there is no battery inserted in the board, the output of the LDO drops below a certain level. I have also checked the input and the input of TP4056-4.2 and observed this behavior reflecting at those points as well. However, when the battery is inserted, there are no issues, and the voltages are stable.
When the LDO is removed, the input and output voltage of TP4056-4.2 is stable.
Please help me to identify the cause of the issue and solution.