Part Number: BQ76952
Hi sir,
when BQ76952 go into shutdown state because of hi temperature 85 degree, which register can I read to know BQ76952 has been in shutdown state.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ76952
Hi sir,
when BQ76952 go into shutdown state because of hi temperature 85 degree, which register can I read to know BQ76952 has been in shutdown state.
Hello Jian,
Reading the voltage level of the TS2 pin should tell if the part is in shutdown or not.
While the device is in SHUTDOWN mode, a ≈5 V level is provided at the TS2 pin with high source impedance. (note that in some cases it will be about 3V due to the high impedance of the TS2 pin, but still shutdown). During normal operation, the TS2 pin should read close to 0V
Regards,
Jose Couso