Part Number: TPS23754
Other Parts Discussed in Thread: PMP6812, TPS23731
Hi all,
I would like to get advice about the most reasonable way to implement redundant power supply for my device by powering it via 2 DC power supplies and 1 PoE as backup.
My end-device needs 12V, 5V and 3.3V voltage outputs and will consume approx. from 3-25 Watts of power.
Both of the DC power supplies provide 12V output voltage. However, power will be consumed from one source - the power from the DC power supplies will be switched via a power MUX e. g. TPS2124Y.
For the PoE design I want to use the TPS23754 and use it with ORing option.
My concerns are:
1. Is it better for this case to use the ORing option 2 and design a flyback converter with 3 output voltages?
2. Or maybe using ORing option 3 and use another dc/dc converter for providing 12V, 5V and 3.3V to my device would be a bettter option?
I have already analysed some of TI's reference designs but anyway I want to make sure that the device will work properly and won't be oversized.
Any help is appreciated!
Best regards, Andrzej