Hello,
I am an FAE for a distributor that handles TI products.
A colleague of mine asked a question in the thread below.
And since I took over the case, I will continue to ask questions in this thread.
In the thread below, my customer confirmed whether changing REG01[3:1] to 111 or 000 changed the behavior.
The result is below.
REG01[3:1] to 111
When the battery voltage is around 3.8V, the charging current repeats ON/OFF periodically.
REG01[3:1] to 000
When the battery voltage is around 2.7V, the charging current repeats ON/OFF periodically.
REG01[3:1] to 101
When the battery voltage is around 3.6V, the charging current repeats ON/OFF periodically.
It seems to have something to do with the SYS_MIN setting.
Is there a way to eliminate the change in charging current?
Best regards,