Hi suppot team,
I would like to know VDO when Io=100mA and 200mA at Vin=15V. The EC table in the datasheet is up to Io=315mA atVin=3V.
Is there a graph for Vin=15V like Figure 6-9 or Iout=200mA and 100mA like Figure 6-10?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi suppot team,
I would like to know VDO when Io=100mA and 200mA at Vin=15V. The EC table in the datasheet is up to Io=315mA atVin=3V.
Is there a graph for Vin=15V like Figure 6-9 or Iout=200mA and 100mA like Figure 6-10?
Hi Kazuya-san,
We don't have the data you requested, but from Figure 6-10 you can see that the dropout voltage does not change once VIN is greater than 4-5V, so you can take Figure 6-9 to represent the case VIN = 15V to a very good approximation.
Regards,
Nick
Hi Nick-san,
Thank you for your reply.
It is an additional question. Is the dropout voltage in Figure 6-9 the maximum value for each Iout?
Furthermore, although Iout=450mA in Fig. 6-10, is the rate of temperature change the same for other current values?
Also, does the same trend apply to voltages above 20V in Figure 6-10? For example, is 30V the same?
Best regards,
Kazuya
Hi Kazuya-San,
Nick is currently OoO. He will return Monday.
Best,
Edgar Acosta
Hi Kazuya-san
The data in all of the Typical Characteristics plots are typical data and not max data. Since this device has a linear dropout voltage vs IOUT curve, a reasonable way to estimate the max for each point is to scale the data to a worst-case. The way I do it is to take the max dropout spec - say 535mV @IOUT=500mA - and calculate a scaling factor. Using Figure 6-9, I would estimate the scaling to be 535/470 = 1.138. Then, the max dropout at 100mA or 200mA can be found from Figure 6-9 by using the 150C curve (i.e. the worst-case dropout curve) and scaling by this factor.
Furthermore, although Iout=450mA in Fig. 6-10, is the rate of temperature change the same for other current values?
No, this is essentially a vertical slice of Figure 6-9 and then swept across VIN. So, you can expect the temperature variation to be lower at lower load currents as in Figure 6-9.
Also, does the same trend apply to voltages above 20V in Figure 6-10? For example, is 30V the same?
Dropout is not defined above VIN = 20V because VOUT is only rated to 18V.
Regards,
Nick
Hi Nick-san,
Thank you for your reply.
This resolved my issue. Thank you very much for helping me.