This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH-POWER-DESIGNER: How Much Can You Edit a Webench Design?

Part Number: WEBENCH-POWER-DESIGNER
Other Parts Discussed in Thread: TPS53647

I miss the old Webench application where you could fully customize your design in the schematic editor.  I want to be able to really go full Frankenstein and experiment with different devices.

I am working on a TPS53647 based design and really want to play with the filtering capacitors on inputs and outputs, different inductors, different power stage devices and even swap between the TPS53647 and TPS54667.

Can't see how I could do that in the current tool.

  • Hi,

    Thank you for the feedback. 

    I am working on a TPS53647 based design and really want to play with the filtering capacitors on inputs and outputs, different inductors, different power stage devices

    I am not sure if I completely understand. However, if you click on the passive component, you could choose an alternate part from the list and re-simulate.

    swap between the TPS53647 and TPS54667.

    Swapping devices on the schematic editor for a particular device is not possible. Let's say inorder to keep the same external components.

    Regards,

    Febin

  • Hi,

    Do you need further support from us?

    If not, I would like to close this thread.

    Regards,

    Febin