This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD95480RWJ: What is RMS current rating?

Part Number: CSD95480RWJ
Other Parts Discussed in Thread: CSD95490Q5MC

What is real RMS current rating of CSD95xxx (CSD95480RWJ and CSD95490Q5MC)?

The brief datasheet is not clear. 

Both devices are showing 70-A/75-A continue current rating.

But TI support said that,

1. 270A is 45A per phase. This is below our continuous rating but still above the RMS rating. This is probably what has caused the failures.

2. On the datasheet, continuous is measured with Ton = 500us. RMS is the true continuous current rating of the device.

T