Hello TI Team!
I have a question about PG function on the Short Circuit condition. (TPS22992S)
Section 9.3.4 Power Good (PG) states that:
Signal The TPS22992x device has a Power Good (PG) output signal to indicate the gate of the pass FET is driven high and the switch is on with the on-resistance close to its final value (full load ready).
Does this mean that in a short circuit condition, the gate of the pass FET is NOT driven high and the state of PG is low?
When exactly does the state of PG change to low?
Do you have an oscillogram of PG in short circuit conditions?
Thank you for your answers!