Actually in TI Document mentioned 61mA by applying VDD =15V AND VEE =-5V , Please confirm how much current required for VEE=-5V supply
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Actually in TI Document mentioned 61mA by applying VDD =15V AND VEE =-5V , Please confirm how much current required for VEE=-5V supply
Hi,
This table is from the safety limiting values table, so these values are the max values to ensure no damage is done to the isolation barrier. This is different from the power supply quiescent current, which is the necessary current the device needs to be operational. The quiescent current values for the VDD and VCC pins can be found in table 6.9, the electrical characteristics table. We don't provide a value for the VEE current because the VEE pin will be outputting current since it's a negative bias pin. Furthermore, this pin has no UVLO (VEE can be zero with no issues) so there isn't a power supply requirement.
Best,
Nancy