Dear sir,
I want to charge Orange 18650 Li-on Battery pack 6 cell , 22.2v, 3c, 10,000mAh by using BQ24650 for 1A charge current, I am using all Resistor capacitor components as per TI datasheet instead of MOSFET Si7288 . When battery get fully charge up to regulation voltage and If I connect or disconnect fully charge battery then BQ24650 IC burn and either LOW side MOSFET or HIGH SIDE MOSFET(IRF7470 used in my My application circuit) get also damaged. To charge 22.2 volt battery and avoid damage charging IC can you suggest components for 22.2v battery charging circuit.
And What is function of Q3, CE bar active low signal in typical application.
I have adjusted MPPT , battery Regulation voltage , As per battery charging 22.2 voltage.