Hi,
We step up the input voltage to VIN of the TPS7A2518DRVR in 25 mV steps, with the EN directly connected to VIN. We then experience that the VOUT voltage starts to rise (from 0V) as VIN reaches ~1.3V. That in itself would not be surprising since VIN is then with margin higher than the 0.9V that is stated as the minimum enable voltage. However, as we continue to step the voltage and pass 1.375V, VOUT goes to 0V again. It then stays there until VIN reases closer to 2.1V.
The load is in single mA range.
Is this expected behavior, or should we keep looking in our system for some other factor generating this behavior?