Part Number: LMZ22010
Other Parts Discussed in Thread: LMZ22008, LMZ23610, LMZ13610
Hi Team,
Is there a recommended part number to P2P replace LMZ22010TZE?
Thank you.
Best Regards
Darren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Darren,
There are a few devices that are pin to pin compatible with LMZ22010 and depending on the application could potentially replace the LMZ22010.
First, if you do not need the full 10A capability you may consider the LMZ22008 or LMZ22006 that are the *A and 6A versions or LMZ22010.
If you need the 10A capability, you can still consider LMZ23610 or LMZ13610, these are providing wider Vin range compared to LMZ22010.
Hope this helps, if so, please set the status of this post to resolved.
Regards,
Yitzhak Bolurian